This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

修改I2C总线路由



使用am437x-evm-linux-sdk-src-03.02.00.05进行移植,硬件参考了am437x-gp-evm但有一些改动。I2C与TI官方开发板不同。.

开发板使用I2C1总线使用T20,T21pin,而我设计的板子使用B13,B14 pin做引脚。

现在修改了am437x-gp-evm.dts

i2c1_pins_default: i2c1_pins_default {
pinctrl-single,pins = <
0x110 (PIN_INPUT_PULLUP | SLEWCTRL_FAST | MUX_MODE2) /* (B13) mii1_rx_er.I2C1_SCL */
0x10c (PIN_INPUT_PULLUP | SLEWCTRL_FAST | MUX_MODE2) /* (B14) mii1_crs.I2C1_SDA */
>;
};

I2C1挂载了24C32的这个设备所有添加了代码

&i2c1 {
status = "okay";
pinctrl-names = "default", "sleep";
pinctrl-0 = <&i2c1_pins_default>;
pinctrl-1 = <&i2c1_pins_sleep>;

24c32@50 {
compatible = "24c32";
reg = <0x50>;

pagesize = <8>;
};
};

仍然无法看到看到设备,并且用示波器抓时数据线,完全没有波形。还需要修改什么地方,是否需要修改UBOOT。