This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 DDR3参数设置问题 (芯片型号MT41K256M16HA-125T)



请教: 我们的应用中,1片C6678外接4片DDR芯片,每片位宽16位。芯片的型号是MT41K256M16HA-125T。由于官方的excel表中没有该款型号,故所有参数均需自己查找DDR芯片手册和C6678手册来配置。现在有一些问题想要求证:

1、时序参数中,tDQSCK应该如何确定?DDR3的SLEW RATE如何设置?

2、DYN_ODT如何设置?

3、该芯片为1600MHz,CL=11.但我们当前并不打算使用这么高的速率,计划降速使用,此时CL仍选取11,还是选择低速对应的值(如1066MHz对应CL=7)?CWL是否也要同步调整?

  • 时序相关的数值在DDR 芯片手册中都可以找到,其他控制配置如SLEW RATE及DYN ODT等可以使用excel中的默认配置;降速的话手册中也应有会根据不同的速率给出不同的配置差异,如你说的CL在1066MHz时则选择7.