This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL138上电启动问题



上个帖子里面提到了1.8V变为2.7V,实际使用中不会出现,我主要问的是上电启动2次才能成功的问题,我这里再重新开个:

一、现象:
1、OMAPL138首次上电出现启动不成功现象无法进入系统,需要在短时间内再次上电才能够启动成功。
2、上电启动成功后采用开关断电进行下电操作,等待1分钟以上后再次上电又会出现上电不成功现象,需要在短时间内再次上电才能够成功进入系统
二、硬件设计:
1、复位电路曾尝试100nf电容、接复位芯片CAT809进行过实验,上电需要2次间隔开关操作才能够启动成功的现象依然存在;
2、排除了外围电路的干扰,设计板上仅包括有OMAPL138、FLASH、DDR2、电源电路以及启动方式选择电路,现象依然存在
3、测试核电压、IO电压等上电顺序,与手册中的一致,首先上电为1.3V核电压之后为1.8V电压最后为3.3V电压

三、目前的解决方式

采用了电容电阻以及与非门芯片搭建了个单脉冲电路,通过控制电源芯片的使能引脚的时序使OMAPL138系统在开机上电4s后进行一次掉电,掉电时间为3s,3s后再次自动上电,这样实现了个二次上电,该方式下开机后系统上电的成功率非常高,我想说的是这个没有从根本上解决问题,希望能够给出一些意见。这个问题使得产品体验效果很差