This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教各位专家,DSP6455的SRIO工作在1X模式,能否这样设计?万分感谢!



各位ti的专家,大家好!

看资料DSP6455的SRIO最高支持3.125GHz,SRIO既支持1个4X或4个1X工作方式,目前我想将DSP6455的SRIO工作在1X模式同时连接4片FPGA,同时工作在3.125GHz的频率,请TI专家指导下,可以这样设计吗?谢谢!

连接器示意图如下: