大家好,我定制了linux内核,发现启动最后显示如下错误,但是系统是可以起来的只是每次都会有一下错误信息:
UBIFS: completing deferred recovery
UBIFS error (pid 971): ubifs_leb_unmap: unmap LEB 9 failed, error -30
UBIFS warning (pid 971): ubifs_ro_mode: switched to read-only mode, error -30
Backtrace:
[<c001876c>] (dump_backtrace+0x0/0x110) from [<c0467438>] (dump_stack+0x18/0x1c)
r6:00000009 r5:ffffffe2 r4:60008401 r3:c0644048
[<c0467420>] (dump_stack+0x0/0x1c) from [<c019bd74>] (ubifs_ro_mode+0x74/0x78)
[<c019bd00>] (ubifs_ro_mode+0x0/0x78) from [<c019c090>] (ubifs_leb_unmap+0x84/0x8c)
r4:c72ed000 r3:c0644048
[<c019c00c>] (ubifs_leb_unmap+0x0/0x8c) from [<c01abd60>] (ubifs_lpt_init+0x1dc/0x460)
r6:0001f000 r5:00000001 r4:c72ed000
[<c01abb84>] (ubifs_lpt_init+0x0/0x460) from [<c0198bac>] (ubifs_remount_fs+0x368/0x638)
[<c0198844>] (ubifs_remount_fs+0x0/0x638) from [<c00b8fe8>] (do_remount_sb+0x9c/0x164)
[<c00b8f4c>] (do_remount_sb+0x0/0x164) from [<c00d1f0c>] (do_mount+0x630/0x6d0)
r7:c72f0e00 r6:c72f0e40 r5:00000000 r4:00124030
[<c00d18dc>] (do_mount+0x0/0x6d0) from [<c00d2290>] (sys_mount+0x8c/0xcc)
[<c00d2204>] (sys_mount+0x0/0xcc) from [<c0014e40>] (ret_fast_syscall+0x0/0x30)
r7:00000015 r6:00000003 r5:beed6cc4 r4:40116afc
xres 480, yres 272, width -1, height -1, 16bpp
set width -1, height -1
PHY: 0:00 - Link is Up - 100/Full