This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SYS/BIOS默认内核中断使用情况

在C6748上使用CCS3.3+DSP/BIOS进行开发,通过DSP/BIOS config的cfg配置文件的图形界面,我们可以观察到DSP/BIOS系统使用了哪些默认的内核中断,见下面截图,使用了T64P0_TINT12,EMU-RTDXRX与EMU-RTDXTX。其中,T64P0_TINT12中断是TIMER0用于驱动操作 系统内核的tick,而EMU-RTDXRX与EMU-RTDXTX应该是仿真器调试时使用。

需要咨询的问题是:

在SYS/BIOS中怎么确认系统默认使用的内核中断与对应的系统事件编号?

这样才好在应用程序的中断使用分配时避开这些系统使用的中断。