This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368接LCD屏幕

想给DM368接一块LCD屏幕显示,请问DM368是否有推荐或者驱动调试好的LCD控制器型号?

谢谢!

  • The digital LCD interface features are described below

    • Programmable DCLK
    • Various output formats
    – YCbCr 16-bit
    – YCbCr 8-bit
    – ITU-R BT. 656
    – Parallel RGB (24 bit)
    – Serial RGB
    • Low-pass filter for digital RGB output
    • Programmable timing generator
    • Master/slave operation
    • Internal color bar generation (100%/75%)
    • 8-bit programable gamma correction

    符合以上信号格式的液晶屏都可以使用

  • 谢谢。

    请问DM368自带的SDK代码中,是否有已经调试好的LCD驱动,可以直接拿来使用?