This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TMS320DM6441仿真器连接失败问题

DSP采用TMS320DM6441,之前的PCB板仿真器连接ARM核和DSP核都正常,但是现在新做的板连接ARM核没问题,连接DSP失败,提示信息如下:

Error connecting to the target:
Error 0x80000240/-275
Fatal Error during: Initialization, OCS, 
This error was generated by TI's USCIF driver.

SC_ERR_SCAN_POLL_BUSY <-275>
The attempt to poll a target device exceeded its timeout limit.
The utility or debugger has requested that a target device be
repeatedly accessed for a specific data or status value.
This has failed because the built-in limit for the maximum number
of attempts when polling the JTAG scan-path has been exceeded.



Board Name: DM6446 XDS560 Emulator
Cpu Name: C6400PLUS_0

Abort: Close Code Composer Studio.
Retry: Try to connect to the target again.
Cancel: Remain disconnected from the target
Diagnostic: Run diagnostic utility.
请问这是什么原因?