This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678多核SPI Boot启动,有时候上电启动后程序会在IPC_Start()出现异常的问题



我们的程序是一个3核程序,使用的是C6678,用SPI Boot启动,程序段放在DDR3上,现在看到的现象是有一块板卡(其他板卡是正常的)有时上电启动后第0核在IPC_Start出现异常,显示为abort() at exit.c;第1,2核程序应该还跑在IPC_Start()没出来;状态截图如下(第2个核跑一下会出现第1核的状态):

请大家帮忙帮忙分析一下可能的原因。

  • 程序放在LL2及SL2有没有问题,是否跟DDR有关,使用ccs JTAG load程序有没有类似的问题。

  • Andy Yin1,您好:

        不好意思,刚看到您的回复,现在这个程序比较大,L2里面装不下,所以还没放到L2试了,DDR的参数我尝试改过,好像没什么影响;我用Load的方式试过,也出现了这样的情况,看后来的输出的打印好像乱了,部分信息如下:

    从23行打印出现了异常,完整的打印的信息附件中;

    麻烦您再帮我们看看是什么原因引起的这个错。