This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PA_emacExample_exampleProject工程遇到问题



我现在使用的是C6678evm平台,调试PA_emacExample_exampleProject工程,启动方式如果选用第一个 NOR boot on image0, 则会报错,错误提示为:

Timeout waiting for reply from PA to Pa_addMac command, 我在论坛上看到很多人遇到这个问题。如果启动方式选择最后一个No boot, 则程序可以正常运行,但如果不执行system reset,重新运行程序,第二次运行也会报错,错误提示同上。所以推测是 Pa_addMac操作不能二次初始化,也就是在选择 NOR boot on image0启动方式时,PA已经初始化了,例程中再次初始化就会报错,而No boot启动方式没有初始化PA,所以第一次程序运行没有问题。我现在的问题是,如果我选择NOR boot on image0,PA已经初始化了,我怎么清除这个初始化而进行自己的初始化呢,也就是不复位板子,只复位PA模块部分,进行后续的初始化问题。


启动方式表: