This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66ak2h PCIe 地址映射问题请教

请问, PCIe的Inbound和outbound可以映射到DDR3A的地址空间,也就是0x8 0000 0000 ~ 0x9 0000 0000这个地址么?如果可以,如何映射,并且,在Linux下如何实现DMA数据拷贝?还有就是memcpy如何数据拷贝?

并且,在Linux下使用mmap函数是,好像不能指定0x8 00000000 ~ 0x9 00000000这个地址段?

另外,请问一下,运行Linux操作系统,使用top命令时,显示系统内存是否包含物理地址 0x8000 0000 ~ 0xFFFF FFFF这段内存空间?