我们目前使用的是OMAPL138处理器,然后在处理器上运行嵌入式Linux系统;在这个平台基础上,我们希望使用蓝牙+WiFi功能。
1、请问我们可以使用什么模块进行操作?
2、考虑过WL1831mod模块,但是这个模块好像只支持AM335X系列,不支持OMAPL138处理器。
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
shine你好,
既然WL1831 暂时用不了;那么如果我们基于OMAPL138处理器运行Linux系统的平台下, 通过OMAPL138处理器控制蓝牙模块,然后可以使用手机、平板的连接通信,这样的话我们可以使用什么蓝牙模块?
1、CC2540 可以支持OMAPL138处理器吗?有运行在Linux平台上的驱动可以使用吗?
2、CC2540与CC2541应该都是可以的吧?
2、如果使用CC2540的话,基于上面的需求情况,应该准备什么硬件、软件才能进行开发?
因为才开始学,好多不懂;谢谢回复。