66ak2h通过usb 3.0链接SSD硬盘,从系统信息看,usb接口速率为5000,但是在Linux写SSD的速率只有60MB/s左右,请问是什么原因?
在PC上测试写入同一个SSD,速率可以到200MB/s以上
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
66ak2h通过usb 3.0链接SSD硬盘,从系统信息看,usb接口速率为5000,但是在Linux写SSD的速率只有60MB/s左右,请问是什么原因?
在PC上测试写入同一个SSD,速率可以到200MB/s以上
看一下CPU负载是多大,USB驱动DMA有没有打开。
K2H是A15的CORE对比PC X86肯定还是弱了些。
你好,CPU占用率基本在100%左右,单核占用率。
另外,请问如何确定usb的dma是否打开了?