我现在在做C6657的IBL,严格按照官方提供的文档来操作,但是目前发现烧写完EEPROM以及FLASH断电重启后,通过示波器观察DSP读完I2C之后并没有去读spi nor flash?挂载仿真器观察电脑指针指到了0x20B00F70、DEVSTAT的值为0x00000001.我之前通过一个简单的不带系统与DDR的闪灯程序验证过SPI的启动方式是可以正常启动的,通过挂载仿真器观测DEVSTAT的值也是按照设定好的spi的boot方式,证明时序应该是没有问题的,不知道为什么会出现这个现象,请各位大神帮帮忙!