在CCS5.5上用XDS100V1连接C5509A,然后将CCS3.3的LED实验转到5.5上运行时出现there are no debuggable cpus问题,求解!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在CCS5.5上用XDS100V1连接C5509A,然后将CCS3.3的LED实验转到5.5上运行时出现there are no debuggable cpus问题,求解!
多谢你的解答,因为是刚接触DSP,而且手上的学习资料都是基于3.3的
我刚刚改了device,然后出现了C55xx: Error connecting to the target: (Error -1146 @ 0x400) Device ID is not recognized or is not supported by driver. Confirm device and emulator configuration is correct, or update device driver. (Emulation package 5.1.73.0)这个问题
配置没什么问题。
是自己的板子吗?量一下JTAG口的各个管脚TCK, TRST, TDI, TDO, TMS, EMU0, EMU1, 是否都正确?