U-Boot# setenv autoload no
U-Boot# dhcp
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
①,u-boot运行以下命令
U-Boot# setenv autoload no
U-Boot# dhcp
后出现下面的情况:
BOOTP broadcast 1
BOOTP broadcast 2
BOOTP broadcast 3
BOOTP broadcast 4
BOOTP broadcast 5
BOOTP broadcast 6
BOOTP broadcast 7
BOOTP broadcast 8
BOOTP broadcast 9
BOOTP broadcast 10
Linux开机时的日志如下:
NAND: 512 MiB
MMC: davinci: 0
Bad block table found at page 262080, version 0x01
Bad block table found at page 262016, version 0x01
In: serial
Out: serial
Err: serial
Net: DaVinci-EMAC
Hit any key to stop autoboot: 0
reading uImage
2403336 bytes read
## Booting kernel from Legacy Image at c0700000 ...
Image Name: Linux-3.3.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2403272 Bytes = 2.3 MiB
Load Address: c0008000
Entry Point: c0008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Booting Linux on physical CPU 0
Linux version 3.3.0 (root@mengzhu-desktop) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #7
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
CPU: VIVT data cache, VIVT instruction cache
Machine: AM18x/OMAP-L138 lcdk board
Memory policy: ECC disabled, Data cache writeback
BUG: mapping for 0x80000000 at 0xfffe0000 out of vmalloc space
DaVinci da850/omap-l138/am18x variant 0x1
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 8128
Kernel command line: mem=32M console=ttyS1,115200n8 root=/dev/mmcblk0p2 rw rootwait ip=off
PID hash table entries: 128 (order: -3, 512 bytes)
Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)
Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)
Memory: 32MB = 32MB total
Memory: 27388k/27388k available, 5380k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
vmalloc : 0xc2800000 - 0xff000000 ( 968 MB)
lowmem : 0xc0000000 - 0xc2000000 ( 32 MB)
modules : 0xbf000000 - 0xc0000000 ( 16 MB)
.text : 0xc0008000 - 0xc0475000 (4532 kB)
.init : 0xc0475000 - 0xc04a0000 ( 172 kB)
.data : 0xc04a0000 - 0xc04d1780 ( 198 kB)
.bss : 0xc04d17a4 - 0xc04eeaac ( 117 kB)
SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:245
Console: colour dummy device 80x30
Calibrating delay loop... 148.88 BogoMIPS (lpj=744448)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
Setting up static identity map for 0xc0362f50 - 0xc0362fa8
gpiochip_add: registered GPIOs 0 to 31 on device: DaVinci
gpiochip_add: registered GPIOs 32 to 63 on device: DaVinci
gpiochip_add: registered GPIOs 64 to 95 on device: DaVinci
gpiochip_add: registered GPIOs 96 to 127 on device: DaVinci
gpiochip_add: registered GPIOs 128 to 143 on device: DaVinci
DaVinci: 144 gpio irqs
print_constraints: dummy:
NET: Registered protocol family 16
EMAC: MII PHY configured
omapl138_lcdk_i2c_init
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c-gpio i2c-gpio.1: using pins 65 (SDA) and 142 (SCL)
Advanced Linux Sound Architecture Driver Version 1.0.24.
Switching to clocksource timer0_1
musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
musb-hdrc musb-hdrc: dma type: dma-cppi41
MUSB255 controller's USBSS revision = 4ea11003
Waiting for USB PHY clock good...
musb-hdrc musb-hdrc: USB OTG mode controller at fee00000 using DMA, IRQ 58
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 1024 (order: 1, 8192 bytes)
TCP bind hash table entries: 1024 (order: 0, 4096 bytes)
TCP: Hash tables configured (established 1024 bind 1024)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.
msgmni has been set to 53
io scheduler noop registered (default)
da8xx_lcdc da8xx_lcdc.0: GLCD: Found VGA_Monitor panel
Console: switching to colour frame buffer device 80x30
Serial: 8250/16550 driver, 3 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO 0x1c42000 (irq = 25) is a AR7
serial8250.0: ttyS1 at MMIO 0x1d0c000 (irq = 53) is a AR7
console [ttyS1] enabled
serial8250.0: ttyS2 at MMIO 0x1d0d000 (irq = 61) is a AR7
brd: module loaded
ahci ahci: forcing PORTS_IMPL to 0x1
ahci ahci: AHCI 0001.0100 32 slots 1 ports 3 Gbps 0x1 impl platform mode
ahci ahci: flags: ncq sntf pm led clo only pmp pio slum part ccc
scsi0 : ahci_platform
ata1: SATA max UDMA/133 mmio [mem 0x01e18000-0x01e19fff] port 0x100 irq 67
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xcc (Micron NAND 512MiB 3,3V 16-bit)
Bad block table found at page 262080, version 0x01
Bad block table found at page 262016, version 0x01
Creating 4 MTD partitions on "davinci_nand.1":
0x000000000000-0x000000020000 : "u-boot env"
0x000000020000-0x0000000a0000 : "u-boot"
0x0000000a0000-0x0000002a0000 : "kernel"
0x0000002a0000-0x000020000000 : "filesystem"
davinci_nand davinci_nand.1: controller rev. 2.5
davinci_mdio davinci_mdio.0: davinci mdio revision 1.5
davinci_mdio davinci_mdio.0: detected phy mask ffffff7f
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[7]: device davinci_mdio-0:07, driver SMSC LAN8710/LAN8720
ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
ohci ohci.0: DA8xx OHCI
ohci ohci.0: new USB bus registered, assigned bus number 1
Waiting for USB PHY clock good...
ohci ohci.0: irq 59, io mem 0x01e25000
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
input: gpio-keys-polled as /devices/platform/gpio-keys-polled.0/input/input0
omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
omap_rtc: RTC power up reset detected
i2c /dev entries driver
watchdog watchdog: heartbeat 60 sec
cpuidle: using governor ladder
cpuidle: using governor menu
davinci_mmc davinci_mmc.0: Using DMA, 4-bit mode
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
usbcore: registered new interface driver snd-usb-audio
ata1: SATA link down (SStatus 0 SControl 300)
soc-audio soc-audio.0: ASoC: Failed to create card debugfs directory
_regulator_get: 1-0018 supply IOVDD not found, using dummy regulator
_regulator_get: 1-0018 supply DVDD not found, using dummy regulator
_regulator_get: 1-0018 supply AVDD not found, using dummy regulator
_regulator_get: 1-0018 supply DRVDD not found, using dummy regulator
asoc: tlv320aic3x-hifi <-> davinci-mcasp.0 mapping ok
ALSA device list:
#0: DA850/OMAP-L138 EVM
TCP cubic registered
NET: Registered protocol family 17
console [netcon0] enabled
netconsole: network logging started
davinci_emac davinci_emac.1: using random MAC addr: 42:d1:89:ad:44:95
omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
Waiting for root device /dev/mmcblk0p2...
mmc0: new high speed SDHC card at address 0002
mmcblk0: mmc0:0002 MSD 7.45 GiB
mmcblk0: p1 p2 p3
kjournald starting. Commit interval 5 seconds
EXT3-fs (mmcblk0p2): using internal journal
EXT3-fs (mmcblk0p2): recovery complete
EXT3-fs (mmcblk0p2): mounted filesystem with writeback data mode
VFS: Mounted root (ext3 filesystem) on device 179:2.
Freeing init memory: 172K
INIT: version 2.88 booting
INIT: /etc/inittab[30]: id field too long (max 4 characters)
davinci_mdio davinci_mdio.0: resetting idled controller
net eth0: attached PHY driver [SMSC LAN8710/LAN8720] (mii_bus:phy_addr=davinci_mdio-0:07, id=)
Starting udev
PHY: davinci_mdio-0:07 - Link is Up - 100/Full
kjournald starting. Commit interval 5 seconds
EXT3-fs (mmcblk0p3): using internal journal
EXT3-fs (mmcblk0p3): recovery complete
EXT3-fs (mmcblk0p3): mounted filesystem with writeback data mode
Starting Bootlog daemon: bootlogd.
ALSA: Restoring mixer settings...
Configuring network interfaces... udhcpc (v1.20.2) started
Sending discover...
Sending discover...
Sending discover...
No lease, failing
done.
Wed Nov 6 16:24:00 UTC 2013
INIT: Entering runlevel: 5
Starting system message bus: dbus.
Starting Dropbear SSH server: NET: Registered protocol family 10
dropbear.
Starting telnet daemon.
Starting syslogd/klogd: done
Starting thttpd.
***************************************************************
***************************************************************
NOTICE: This file system contains the followin GPLv3 packages:
gdbserver
If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
Stopping Bootlog daemon: bootlogd.
umount: can't umount /mnt/.psplash: Device or resource busy
②,然后,我们运行了starterware中enet_echo例程;
在ti烧写了Linux的开发板上,用ccs运行正常。
而在自己的开发板上,卡在lwIpInit()函数的while循环位置,如下图。
函数中长时间卡在以下位置: