我使用6478做udp通讯,但调用udp_sendto时返回ERR_VAL,进入函数内部发现是
if (ip_addr_isany(&pcb->local_ip)) {
/* use outgoing network interface IP address as source address */
src_ip = &(netif->ip_addr);
} else {
/* check if UDP PCB local IP address is correct
* this could be an old address if netif->ip_addr has changed */
if (!ip_addr_cmp(&(pcb->local_ip), &(netif->ip_addr))) {
/* local_ip doesn't match, drop the packet */
if (q != p) {
/* free the header pbuf */
pbuf_free(q);
q = NULL;
/* p is still referenced by the caller, and will live on */
}
return ERR_VAL;
}在这段代码处报错,不知道是怎么回事?