This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678调试SRIO例程出错



我是个DSP新手,还没入门,用6678的EVM调试SRIO ,例程为网上下载的Keystone例程,调试出现下面的情况:

Enable Exception handling...

External exception happened. MEXPFLAG[3] = 0x200000.

    Event 117: UMC_ED2 Uncorrected bit error detected

    Enter LL2 EDC handler, but no error flag is set!

NRP=0xc046cf8, NTSR=0x1000d, IRP=0x0, ITSR=0x0, TSCH=0x0, TSCL=0x42066

  B3=0xc046c94, A4=0x1, B4=0x3, B14=0x8254c8, B5=0x8231d8

SRIO_DIGITAL_LOOPBACK test start................................................................................................

Initialize DSP main clock = 100.00MHz/1x10 = 1000MHz

Initialize DDR speed = 66.67MHzx/1x20 = 1333.333MTS

DDR3 leveling has failed, STATUS = 0x40000064

请教一下这是什么原因导致的?应该怎么解决?