This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

基于FMC标准的1路CameraLink Full输入、1路HDMI输出子卡模块



          FMC202是北京青翼科技研发的一款基于FMC接口标准的1路CameraLink Full模式(或者2路CameraLink Base模式)采集、1路HDMI(DVI)视频输出的子卡模块,该模块具有2个CameraLink端口(SDR,26PIN),可通过硬件配置成1路Full输入或者2路Base模式输入,CameraLink接口支持80Bit Deca模式(即Full Plus模式)。该模块支持1路DVI视频输出(HDMI连接器),最大支持1080P分辨率。

         该模块专门为FMC夹层卡设计,通过搭配不同的FMC载卡,可快速搭建起基于CameraLink视频接口的影像分析验证平台。可广泛应用于教学科研和高端视频图像产品的研制。

 技术指标

图像接口性能

 1.支持2路CameraLink Base数字相机输入;

2.支持1路CameraLink Full模式输入;

3.支持80bit Deca(Full Plus)模式,最大传输带宽850MByte/s;

4.2个SDR26连接器,型号为12226-5150-00FR;

5.支持1路DVI数字显示输出,最大支持1920x1080分辨率。

6.1个HDMI接口,型号为:10029449-001RLF;

7.DVI驱动芯片:TFP410PAP,最大像素时钟165MHz;;

FMC接口指标

1.标准FMC子卡,符合VITA57.1规范

2.板卡尺寸:84.1 x 69 mm,增强型导冷框架;

3.FMC连接器型号:ASP-134488-01;

4.板卡采用+3.3V供电;

5.CameraLink的3组信号线X/Y/Z等长设计;

6.支持IIC接口;

 其它接口:

1.1个RS422/RS485/RS232多协议接口;

2.8个GPIO输入/输出;

3. 8个LED指示灯;

软件支持

1.可选集成板级软件开发包(BSP):

2. 底层接口驱动:CameraLink接口、DVI接口;

3. 板级互联接口驱动;

4. 可根据客户需求提供定制化算法与系统集成:

应用范围

1. CameraLink影像分析;

2. 高清视频传输与处理;

3.医学影像分析处理;