This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AIF时钟信号是怎么获取的



打算用fpga和aif互联,做一个远端环回的测试,先从dsp发给fpga,然后fpga发回给dsp,使用cpri协议,单link 8x,

现在dsp接收侧经常失步,检测到los 一直在涨,怀疑时钟有问题

1 aif的接收方向的时钟是是从rx恢复出来的还是从本地时钟获取的?

2 Serdes 时钟频率的配置具体是通过哪些寄存器的配置做到的?ti安装目录里的例子中有个k2的宏,解开后是否能自动配置

3 我打开了aifclock qulaity的功能,设置mon wrap为100,检测到clk qual是84,那么 byte clock的频率是100/84x245.76 =292MHZ

292Mhz x 8倍速率 为 2.336Ghz 这个值是否正确