This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368显示屏移植



我们手里有DM368的视频采集与显示系统,显示部分连接3.5寸屏,型号是LQ035NC111.

使用CCIR656编码,目前工作正常。下面是硬件连接图纸

因为项目需要想更换成大尺寸的显示屏,初步预定8寸左右。

目前其他硬件接口已经被占用,想在现有的3.5寸屏基础上进行修改,请问应该从哪个地方着手?

  • 你好,

    你的意思是,目前LCD输出接口只能使用8根数据线?如果是,你需要找到一个符合接口要求的大屏。

    如果dm36x的VPFE的pclk输出超过27M,就需要外部时钟输入,这点也需要注意。具体信息请参考数据手册对EXTCLK的描述:

    Video Encoder: External clock Input, used if clock
    rates > 27 MHz are needed, e.g. 74.25 MHz for
    HDTV digital output.