This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP运行异常?打印出 [C66xx_0] A0=0x0 A1=0x0 [C66xx_0] A2=0x0 A3=0x8052e27a......

Other Parts Discussed in Thread: SYSBIOS

    我的DSP程序运行DDR3,开始使用SPI boot,大部分上电是正常的,有时上电加载后程序出现出现异常,后来我用load的方式调试,发现了异常,打印信息如下:

[C66xx_0] Configuring CPSW ...Done
[C66xx_0] A0=0x0 A1=0x0
[C66xx_0] A2=0x0 A3=0x8052e27a
[C66xx_0] A4=0x9 A5=0x42a
[C66xx_0] A6=0x0 A7=0xffffffff
[C66xx_0] A8=0x80533c30 A9=0x0
[C66xx_0] A10=0x0 A11=0x80533c30
[C66xx_0] A12=0xdfc957de A13=0xadeba7e7
[C66xx_0] A14=0x0 A15=0xff9dbeff
[C66xx_0] A16=0x7fffffff A17=0x7025930d
[C66xx_0] A18=0x80546db0 A19=0xf4e9fbef
[C66xx_0] A20=0x80472970 A21=0x718400
[C66xx_0] A22=0x0 A23=0x42400800
[C66xx_0] A24=0x80543720 A25=0x1
[C66xx_0] A26=0x80543714 A27=0x80543704
[C66xx_0] A28=0x8054371c A29=0x8054370c
[C66xx_0] A30=0x80543718 A31=0x80543724
[C66xx_0] B0=0x1 B1=0x8054372c
[C66xx_0] B2=0x80543708 B3=0x80543728
[C66xx_0] B4=0x805436f8 B5=0x80543700
[C66xx_0] B6=0x9 B7=0x1
[C66xx_0] B8=0x9 B9=0x1
[C66xx_0] B10=0x805436f0 B11=0x8052f6fa
[C66xx_0] B12=0x80543690 B13=0x80436dc4
[C66xx_0] B14=0x805436e0 B15=0x1e
[C66xx_0] B16=0x30 B17=0x8048f9e0
[C66xx_0] B18=0x2 B19=0x80543698
[C66xx_0] B20=0x805436e8 B21=0x1
[C66xx_0] B22=0x805436ec B23=0x805436f4
[C66xx_0] B24=0x8052f77d B25=0x80543610
[C66xx_0] B26=0x8048cebc B27=0xdfffff77
[C66xx_0] B28=0xffff5f7f B29=0xf5bf2bfb
[C66xx_0] B30=0x79f70000 B31=0x80543620
[C66xx_0] NTSR=0xffffffff
[C66xx_0] ITSR=0xffffffff
[C66xx_0] IRP=0xfffffff7
[C66xx_0] SSR=0x37666666
[C66xx_0] AMR=0x36363733
[C66xx_0] RILC=0x0
[C66xx_0] ILC=0x0
[C66xx_0] Exception at 0x0
[C66xx_0] EFR=0x2 NRP=0x0
[C66xx_0] Internal exception: IERR=0x1
[C66xx_0] Instruction fetch exception
[C66xx_0] ti.sysbios.family.c64p.Exception: line 255: E_exceptionMin: pc = 0x00000000, sp = 0x00000010.
[C66xx_0] To see more exception detail, use ROV or set 'ti.sysbios.family.c64p.Exception.enablePrint = true;'
[C66xx_0] xdc.runtime.Error.raise: terminating execution

从第二句开始是异常打印信息,这段打印是什么意思?什么情况下会出现这种打印?大家帮忙分析。