This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于 AMIC 110 GPIO口 灌电流 问题



手册中有这样子的描述,当VDDSHVx接3.3V时,图中IOL = 6mA 是否 为 GPIO可以忍受的灌电流?  如果是 那么多问题来了,现在我打算接32路 IO口,每一路灌电流大约为4.5mA,如果32路同时打开,那么就会有  32路的 4.5mA 电流,此时GPIO能否承受? 是否需要加 类似于 74LVC244 之类的缓冲器。