想用示波器看SRIO的波形眼图,但只有一个6678EVM开发板,所以想短接两个port,例如SRIO配置成1xlaneA_1xlaneB,AB端口短接,看论坛中以前的问答说不行,是指当前论坛提供的例程不支持(发送端程序烧到dsp0的core0,接收端烧到DSP1的core1),还是本身硬件不支持这种配置?如果是硬件不支持,是哪些寄存器配置时冲突了,想知道原理。请问有没有1x1x短接的例程?有没有只一块EVM用示波器看SRIO波形的方法?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
想用示波器看SRIO的波形眼图,但只有一个6678EVM开发板,所以想短接两个port,例如SRIO配置成1xlaneA_1xlaneB,AB端口短接,看论坛中以前的问答说不行,是指当前论坛提供的例程不支持(发送端程序烧到dsp0的core0,接收端烧到DSP1的core1),还是本身硬件不支持这种配置?如果是硬件不支持,是哪些寄存器配置时冲突了,想知道原理。请问有没有1x1x短接的例程?有没有只一块EVM用示波器看SRIO波形的方法?
您可以用BOC卡链接2个66X的EVM板子,自己飞线的话,因为SRIO是高速信号,可能信号完整性不能保证,这样测试就没有意义了,当然你可以试试。代码做少许改动即可,可以1个COER做发送,另外1个CORE做接收
感谢Thomas!
硬件连接时A的发送连接A的接收就可以吧?
没这样链过,你可以试试。首先看LINK可不可以UP起来