在CCS6.2的帮助中,发现如下中断配置例程:
Int eventId; Hwi_Params params; Error_Block eb; // Initialize the error block Error_init(&eb); // Map system interrupt 15 to host interrupt 8 on Intc 0 CpIntc_mapSysIntToHostInt(0, 15, 8); // Plug the function and argument for System interrupt 15 then enable it CpIntc_dispatchPlug(15, &myEvent15Fxn, 15, TRUE); // Enable Host interrupt 8 on Intc 0 CpIntc_enableHostInt(0, 8); // Get the eventId associated with Host interrupt 8 eventId = CpIntc_getEventId(8); // Initialize the Hwi parameters Hwi_Params_init(¶ms); // Set the eventId associated with the Host Interrupt params.eventId = eventId; // The arg must be set to the Host interrupt params.arg = 8; // Enable the interrupt vector params.enableInt = TRUE; // Create the Hwi on interrupt 7 then specify 'CpIntc_dispatch' // as the function. Hwi_create(7, &CpIntc_dispatch, ¶ms, &eb);
这里 myEvent15Fxn 为自定义函数,CpIntc_dispatch 为内部函数,当系统中断事件发生时,应该会执行myEvent15Fxn,
那么将 Host interrupt 再关连到硬件中断7的作用是什么,如果不关连就是不会执行 myEvent15Fxn吗?
既然已经指定中断服务函数 myEvent15Fxn,CpIntc_dispatch作用是什么?