This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6678性能验证VLFFT的疑问



专家您好!我想问您的是:现在我在用您所提供的例子VLFFT做性能验证,总是出现错误的警告,而且在工程里没有源文件的存在,是不是这个例子需要特定版本的软件支持才可以?麻烦请您指出需要什么版本,我现在安装的是CCS Version 5.1.0.08020

 下面是出现的几个警告,麻烦您给指导一下:

    RTSC product 'MCSDK' V2.0.0.11(or equivalent) is not currently installed    (是不是说明我的MCSDK版本不对,我安装的是最新版本的)

   A compatible version 2.1.0.3 has been used ,please install a product of equivalent version or enable one of the supported version of this product

  this project contains unresolved buildable linked resources,it might not build as expected

this project was created using a version of compiler that is not currently installed;7.3.1[C6000],please install the compiler of this version ,or migrate the project to one of the supported version

是不是MCSDK,以及SYS/BIOS都需要特定的版本才可以?还要对提供的例程做修改吗?麻烦您了,谢谢!