Other Parts Discussed in Thread: AM3505, AM3517
X-Loader 1.51
U-Boot 2010.06
Linux version 2.6.37
CPU:AM3505
以上是我的开发环境,请问怎样修改u-boot,使之支持ubifs?我已经配置了kernel,使之支持ubifs。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
processors.wiki.ti.com/.../UBIFS_Support
这个网页没有介绍u-boot支持ubi的移植方法
在u-boot/include/configs/am3517_evm.h中加上以下定以后,nand驱动有问题
#define CONFIG_MTD_DEVICE 1
#define CONFIG_MTD_PARTITIONS 1
Hit any key to stop autoboot: 0
环境变量如下:
AM3517_EVM # pri
bootcmd=if mmc init; then if run loadbootscript; then run bootscript; else if run loaduimage; then run mmcboot; else run nandboot; fi; fi; else run nandboot; fi
bootdelay=1
baudrate=115200
bootfile=uImage
loadaddr=0x82000000
console=ttyO2,115200n8
mmcargs=setenv bootargs console=${console} root=/dev/mmcblk0p2 rw rootfstype=ext3 rootwait
nandargs=setenv bootargs console=${console} root=/dev/mtdblock4 rw rootfstype=ubifs
loadbootscript=fatload mmc 0 ${loadaddr} boot.scr
bootscript=echo Running bootscript from mmc ...; source ${loadaddr}
loaduimage=fatload mmc 0 ${loadaddr} uImage
mmcboot=echo Booting from mmc ...; run mmcargs; bootm ${loadaddr}
nandboot=echo Booting from nand ...; run nandargs; nand read ${loadaddr} 280000 400000; bootm ${loadaddr}
mtdparts=nandflash0:0x80000@0x0(x-loader),0x240000@0x80000(u-boot),0x280000@0x240000(u-boot-envl),0x780000@0x280000(kernel),0x3980000@0x78000(ubifs),-(jffs2)
stdin=serial
stdout=serial
stderr=serial
dieid#=32ea00010000000001608a901200a014
Environment size: 997/131068 bytes
打印nand信息,没有任何输出
AM3517_EVM # nand info
AM3517_EVM #
擦出nand的ubifs分区,提示没有可用的设备
AM3517_EVM # nand erase ubifs
no devices available
AM3517_EVM #