我现在需要在C6678的core0使用GPIO1的中断,但是我看C6678的数据文档发现不好实现,相关文档信息如下:
在TMS320C6678 System Event Mapping — C66x CorePac Primary Interrupts表格中只有GPI08~15,还有GPINTn,也就是GPIO1只能由core1接收中断;文档图如下:
在中断拓扑图中,0核中断间接也只能由CLC0输入,而CLC0中没有看到和GPIO1相关的事件,中断拓扑图如下:
唯一和GPIO1事件相关的是CLC3,而CLC3接的是HyperLink 和EDMA3CC0 ;
我现在的问题有两个:
1.GPIO1是不是没办法中断连接到core0,我现在理解的对不对?
2.如果core0想使用GPIO1中断,有没有其他变通的方法?