请问下大家,DM8107上,HDMI输出有没有相应的图层进行osd显示,比如可以用一些gui显示菜单等。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问下大家,DM8107上,HDMI输出有没有相应的图层进行osd显示,比如可以用一些gui显示菜单等。
我看了下,加载ti81xxfb.ko驱动后,dev下生成了三个fb,这样我就可以按照普通的方式操作framebuf了吗?还有我如果访问HDMI/dvo1输出的framebuf,就是fb0,dvo2的就是fb2,这样理解对吗?还有就是我要开机logo,我可以直接通过a8来控制输出吗?谢谢能给我一些建议。
你好;
framebuffer 默认是这样配置的;
可以自己配置,在 mcfw/src_bios6/links_m3vpss/system/system_dctrl.c 文件中
配置 gSystem_dctrlTriDisplayConfig 中的 VPS_DC_GRPX0_INPUT_PATH 的绑定通道;
具体可以参考 hdvpss 的相关文档。
我按照hdvpss文档,可以在hdmi输出的osd上可以显示了,我现在想dvo2 也就是vout0上链接了lcd,我按照手册的不能直接加载ti81xxvo.ko,但是可以把vpss驱动改成insmod /opt/ipnc/kermod/vpss.ko tiedvencs=4 sbufaddr=0xbfb00000后,可以加载,我想问下ti81xxhdmi驱动不包括DVO2的驱动吗?