This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 DEMA中PaRAM参数配置问题



您好,TI工程师:

程序中创建测量数据,DDR3的首地址为0x80000000

int *pddr3=(int *)DDR3_BASE

for(i=0;i<8;i++)

{

      pddr3[i]=i;

}

程序中配置了一个一维8个元素的数组。

而在EDMA传输数据时,传输数据的维数是否可由PaRAM决定呢?如上述数据

是否可通过PaRAM配置成Acnt=4,Bcnt=4,Ccnt=2,配置成2X4的数据??也就是说PaRAM能够配置数据的维数?传输数据的维数是由pddr3[i]决定还是由PaRAM配置?

希望得到您的回答,谢谢!

  • EDMA传输的维数由Acnt, Bcnt, Ccnt决定。

    你配的Acnt=4,Bcnt=4,Ccnt=2,应该是配置成4x4x2的数据。具体可以参考user guide。

    2.2 Types of EDMA3 Transfers
    http://www.ti.com/lit/ug/sprugs5b/sprugs5b.pdf