This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM437x ADC0用于模拟量采集出错



大家好,

       我用AM437x ADC0的 0/1/2/3用做4线电阻触摸屏,4/5/6/7用作模拟量输入,LINUX用的是TI官网下载的4.1.y内核SDK包。触摸屏能够正常工作,但任选一个模拟输入通道接入1.25V(输入电压已绕过中间电路,相当于直接接到了CPU的PIN上,另外我的VDDA参考电压为1.225V),读取寄存器原始数值大概在2560(十进制)左右,并且波动值为10左右,始终无法到4095附近,请问会是哪里的问题?谢谢