This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP5509A USB驱动安装问题



芯片型号:5509A

CCS版本:4.1.2

问题描述:本人电脑是用window7 64位的操作系统,开发板的USB直接连在DSP5509A芯片管脚上:

现在的问题是:在window7环境下安装不了USB驱动,下载不了程序(本人没有仿真器,所以选择直接讲程序下载到芯片中)请各位技术大师给我提供一个DSP5509A在window7  64位环境下的USB驱动,谢谢!

  • 你好,首先CCS 4.1.2对DSP芯片进行程序仿真下载时候,是通过JTAG口进行的。如果是想直接从USB口下载程序到DSP RAM去运行,肯定需要第三方软件工具,这个工具也肯定不是CCS。所以寻找DSP5509A在window7  64位 CCS环境下的USB驱动,目前没有发现。