This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6657 spi boot问题



大家好:

  我使用的是c6657.

  1.我使用发表在www.deyisupport.com/.../100597.aspx的Keystone 1 SPI NOR 方法步骤,可是实现单核boot。

  2.目前使用双核boot,在使用工具b2i2c.exe时显示Max input array size exceeded,然后在论坛www.deyisupport.com/.../47726.aspx中 提供的b2i2c.c使用VC++6.0重新生成工具使用,不会跳出提示。

  3.在进行到使用romparse.exe时,提示出现一个问题,导致程序停止正常工作,不能正常生成i2crom.ccs。请问这一步该如何操作?

  4.可否上传一份较为支持文件较大点的完整工具链。

谢谢