This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6657的UART0不能收发问题



问题描述:

1.UART0和UART1均配置为无校验,采用中断方式;UART0用于与上位机通讯,UART1用于与传感器通讯。

2.问题1简单描述:当C6657串口配置为无校验时,如果上位机采用奇校验或者偶校验方式发送命令时,串口立刻死机

3.问题1详细描述:保证串口接通的情况下,当上位机故意操作,先采用奇校验方式对UART0发送命令时,UART0出现死机现象,即不能进入接受中断;且即使更换为无校验方式时,再次发送指令UART0仍然不能进入接受中断。

4.问题2:在线仿真时,串口用于与传感器通讯,因先上电传感器就开始发送数据,此时再次连接C6657内核仿真时,串口死机,不能正常进入收发中断。即必须先连接上C6657,之后串口再有数据来时才不会有问题