This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148平台RDK,A8上通过ipcbitsoutlink发送码流出错。



您好!

     我们在使用dm8148时,发现有些芯片上我们的程序经常出现ringbuffer写失败的问题:

ringbuffer的状态如下:


[RingBuf]
********** RingBuf - 0 Info (378, RingBufferWriterAcquire) ***********

[RingBuf] initDone :TRUE
[RingBuf] base :0x4C4A5B00
[RingBuf] totalSize :10368000
[RingBuf] availSize :10368000

[RingBuf] Writer -> acqPtr[1572864] acqSize[1553280] relPtr[19584] relSize[0]
[RingBuf] Reader -> acqPtr[19584] acqSize[0] relPtr[19584] relSize[8814720]
[RingBuf] Count -> writer [932059, 932059, 932058] reader [932059, 932059, 0]

[host] RingBuf(379, RingBufferWriterAcquire) - Writer: Acquire already done

這里很奇怪,writecancelcount的次数竟然比writereleasecount要少一次,而reader却等于writer。似乎ringbufferwritercancel少了一次调用,但是代码里面确实是调用了。

 

  • chao fan2 说:
    有些芯片上我们的程序经常出现ringbuffer写失败的问题

    同样的软件,只有部分的板子上有下面的问题?

    如果是,是否有尝试过降低DDR频率,看是否有改善?出问题的板子的电源是否有测量过电压/纹波等是否满足要求?