This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6678 boot问题



您好,

我们正在调试自制的板子,dsp用的是6678。

1,我们自制板子硬件引脚配置为spi模式,请问使用spi向nor flash(用nor writer工程)烧程序时,必须要先配置为no boot模式吗?

2,我的ddr和开发板不同,那我如何修改gel文件?或者我烧录时不用gel文件,在nor writer程序中开始加上DDR 初始化,可以吗?

谢谢各位的回答!

  • 1.工程烧写时与硬件引脚配置为何种模式无关,只要你能连上片子,烧就行了。

    2.首先我用搞DSP大概有十年了,从来不用gel文件,不要问为什么,就是感觉不好用。烧写为何要初始化DDR?一般DDR初始化放在二级bootloader里。

  • 1.不用配置为no boot模式

    2.gel文件中的DDR配置与你在裸跑是配置DDR的方式一样,都是参考DDR配置的两个表格,生成相应的参数,使用文本编辑器打开gel文件,找到配置DDR的函数,对参数进行修改就好了。

    3.对于你说的不使用gel文件,修改norwriter程序,我当初也想到使用这种方法,但是修改后发现,程序无法load,可能与cmd文件有关,最后还是使用的是修改gel文件,如果你不想修改gel文件,不嫌麻烦的话,你可以先load你当前的工程,使其运行到DDR初始化后,不断电,然后再去烧写你的程序