This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678连不上仿真器的问题。(POR和RESETFULL不受控制)



 我两片板子DSP都连不上仿真器。现象都一样。单板是FPGA + DSP 的架构。FPGA是K7325T,DSP就是6678。FPGA和DSP 的上电时序都用CPLD控制了。实际测量也满足DSP时序要求。检查6678的POR和RESETFULL这两个信号,发现这连个信号不受控制。(DSP的三个复位都由K7325T控制,确认K7逻辑无误,绑定的管脚无误)。设置POR比RESERFULL先上20ms,实际测量这两个信号一起上电。因该是这个引起的DSP JTAG连不上。请教各位大神专家该怎么办,调了两天也没进展。DSP已经工作,测量SYSCLKOUT为16.66M,内核时钟供的100M。小弟先谢谢大家了,项目很急,卡在DSP JTAG这了。