- 你好,我们用的芯片是dm8168, yuv视频数据通过dma 给到内存,再去编码。现在有个问题,视频数据通过dma过来,存储下来看没有问题。但是只要编码,存储下来的dma过来的yuv视频数据会花屏,所以请问一下,dm8168 在编码和dma共同工作的时候,他们之间有什么影响吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
补充一下,dm8168是rc模式,外围挂载的ep设备通pcie dma数据到dm8168的共享内存中。编码处理器编码此共享内存中的数据。
你好,
两者都会访问DDR,会使用DDR的带宽资源。
如果减慢PCIE传输的速度,或者减少编码的码率/分辨率,对问题有改善么?
降低DDR运行频率是否有改善?
你好,我现在ddr的工作频率已经降到400m,视频现在是彩条测试数据,码率大概只有500kbps,参数设置的是2000kbps。