尊敬的TI工程师:
您好,现在我用GPIO模拟串口UART。想用GP22作为输出,但是这个IO口输出的速率很慢,10hz一下的输出方波的波形正常,让它以1Khz,它就成一条直线了,输出的全是高电平。我哪里设置错了?
/* Disable CPU interrupt */ IRQ_globalDisable(); /* Initialize Interrupt Vector table */ IRQ_setVecs((Uint32)(&VECSTART)); /* Open GPIO module */ hGpio_GP22 = GPIO_open(&GpioObj_GP22,&status); GPIO_reset(hGpio_GP22); config.pinNum = CSL_GPIO_PIN22; config.direction = CSL_GPIO_DIR_OUTPUT; config.trigger = CSL_GPIO_TRIG_CLEAR_EDGE; status = GPIO_configBit(hGpio_GP22,&config);
/* Enabling Interrupt */
IRQ_enable(GPIO_EVENT);
IRQ_globalEnable();
void gpt1Isr(void)
{
fTimer_01++;
if(fTimer_01%2 == 0)
{
GPIO_write(hGpio_GP22,CSL_GPIO_PIN22,1);
}
else
{
GPIO_write(hGpio_GP22,CSL_GPIO_PIN22,0);
}
/* Clear Timer Interrupt Aggregation Flag Register (TIAFR) */
CSL_SYSCTRL_REGS->TIAFR = 0x02;
printf("\r\nTimer1 ISR\r\n");
}