官网上的下不下来
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ccs3.3停产了,所以很多跟它相关的链接失效了。
你现在的问题是在ccs3.3里找不到合众达仿真器的dm6467驱动吗?有没有更新过ccs.3版本的合众达仿真器驱动程序?
驱动程序找得到,但就是连接不上
出现错误
Error:
Error 0xA0002020/-114
Error during: Execution, Control,
This error was generated by TI's USCIF driver.
SC_ERR_OCS_BUSY <-114>
The controller's commands are taking too long to complete.
This often implies one of the following errors:
1. The target cable is disconnected near-to the controller.
2. The target cable is disconnected far-from the controller.
3. The target system has lost its JTAG clock.
4. The target system has lost its power supply.
5. The controller is in an invalid state and should be reset.
下面框体中还出现Warning: 0x40003200/-1014 @ marker 10700 Warning during: OCS, Target, Control, PTI_ERR_ICE_STATUS Error Occured at 0x000029CC
http://downloads.ti.com/dsps/dsps_registered_sw/sdo_ccstudio/CCSv3/CSPS/DM6467_CSP_v3.3.1007.EXE
这个资源确实有点问题;