This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于dvo 输出标清信号送到lcd



目前,lcd已经确认工作,并且framebuf,可以输出到lcd,遇到问题,就是怎么送出视频,我只是改了capturedisplay的 

  gVdisModuleContext.displayId[VDIS_DEV_HDMI] = SYSTEM_LINK_ID_DISPLAY_1;

displayPrm.displayRes = VSYS_STD_480I ;//gVdisModuleContext.vdisConfig.deviceParams[VDIS_DEV_HDMI].resolution;//VSYS_STD_720P_60
displayPrm.displayId = DISPLAY_LINK_DISPLAY_BP1;还需要修改其他吗,我们想让输出8bit 的656格式。

  • 你好,

    请你使用的芯片型号是?使用的软件版本是?

    BT656是内同步,8bit,你是否有在linux侧配置相关参数?

    http://processors.wiki.ti.com/index.php/TI81XX_PSP_VPSS_Video_Driver_User_Guide

    请注意下面的勘误,如果你VOUT1要输出BT656,那同时HDMI是不能正常输出的。

    Advisory 3.0.23 HDMI: On-Chip HDMI Does Not Operate in 8-/16-bit Mode

  • 谢谢你的回答,我们的屏幕是连接在dvo2 上的也就是vout0上,并不是dvo1上,应该是和hdmi独立的,我们想通过dvo1 输出到lcd上。我不是很明白,ipnc3.8里的sd vensc是说的analog TV吧,我们连接到dvo2需要标清的信号和这个有关系吗?dvo2可以通过vout0直接输出标清信号吗?那我需要怎么指定displayid和修改gSystem_dctrlTriDisplayConfig(方案历史hdmi和HDCOMP绑定一起的,意思是他们必须输出相同内容吗?)的配置。谢谢你能给我些帮助。

  • 我们使用的是dm8107

  • 你好,

    你是否有参考过下面的讨论:

    https://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/p/408435/1456021