使用场景是一片C6416和一片C6713通过McBSP相连接
C6416配置McBSP为SPI主模式,C6713配置McBSP为SPI从模式
C6416一直进行数据发送,但是C6713的rrdy一直没有信号,也就是无法读取SPI的DRR数据
用示波器测量了C6416的时钟、片选、数据,都是正常的
请问这是什么问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用场景是一片C6416和一片C6713通过McBSP相连接
C6416配置McBSP为SPI主模式,C6713配置McBSP为SPI从模式
C6416一直进行数据发送,但是C6713的rrdy一直没有信号,也就是无法读取SPI的DRR数据
用示波器测量了C6416的时钟、片选、数据,都是正常的
请问这是什么问题?
C6416的McBSP配置如下
void init_mcbsp(MCBSP_Handle handle) { Uint32 spcr, rcr, xcr, srgr, mcr, pcr; Uint32 rcere0, rcere1, rcere2, rcere3; Uint32 xcere0, xcere1, xcere2, xcere3; /* SPI mode, CLKSTP = 11b and CLKXP = 0: Clock starts with rising edge with delay. */ spcr = MCBSP_SPCR_RMK( MCBSP_SPCR_FREE_DEFAULT, MCBSP_SPCR_SOFT_DEFAULT, MCBSP_SPCR_FRST_DEFAULT, MCBSP_SPCR_GRST_DEFAULT, MCBSP_SPCR_XINTM_DEFAULT, MCBSP_SPCR_XSYNCERR_DEFAULT, MCBSP_SPCR_XRST_DEFAULT, MCBSP_SPCR_DLB_DEFAULT, MCBSP_SPCR_RJUST_DEFAULT, MCBSP_SPCR_CLKSTP_DELAY, /* CLKSTP = 11b */ MCBSP_SPCR_DXENA_OFF, MCBSP_SPCR_RINTM_DEFAULT, MCBSP_SPCR_RSYNCERR_DEFAULT, MCBSP_SPCR_RRST_DEFAULT ); rcr = MCBSP_RCR_RMK( MCBSP_RCR_RPHASE_SINGLE, MCBSP_RCR_RFRLEN2_DEFAULT, MCBSP_RCR_RWDLEN2_DEFAULT, MCBSP_RCR_RCOMPAND_DEFAULT, MCBSP_RCR_RFIG_NO, MCBSP_RCR_RDATDLY_1BIT, /* 1 - (Master) */ MCBSP_RCR_RFRLEN1_DEFAULT, MCBSP_RCR_RWDLEN1_32BIT, MCBSP_RCR_RWDREVRS_DISABLE ); xcr = MCBSP_XCR_RMK( MCBSP_XCR_XPHASE_DEFAULT, MCBSP_XCR_XFRLEN2_DEFAULT, MCBSP_XCR_XWDLEN2_DEFAULT, MCBSP_XCR_XCOMPAND_DEFAULT, MCBSP_XCR_XFIG_DEFAULT, MCBSP_XCR_XDATDLY_1BIT, /* 1 - (Master) */ MCBSP_XCR_XFRLEN1_DEFAULT, MCBSP_XCR_XWDLEN1_32BIT, MCBSP_XCR_XWDREVRS_DISABLE ); srgr = MCBSP_SRGR_RMK( MCBSP_SRGR_GSYNC_FREE, MCBSP_SRGR_CLKSP_RISING, MCBSP_SRGR_CLKSM_INTERNAL, /* SRGR clock mode from internal source */ MCBSP_SRGR_FSGM_DEFAULT, MCBSP_SRGR_FPER_DEFAULT, MCBSP_SRGR_FWID_DEFAULT, MCBSP_SRGR_CLKGDV_OF(0) /* C64X: CLKG = CPU/4 / (CLKGDV+1) */ ); mcr = MCBSP_MCR_DEFAULT; rcere0 = MCBSP_RCERE0_RMK(0); rcere1 = MCBSP_RCERE1_RMK(0); rcere2 = MCBSP_RCERE2_RMK(0); rcere3 = MCBSP_RCERE3_RMK(0); xcere0 = MCBSP_XCERE0_RMK(0); xcere1 = MCBSP_XCERE1_RMK(0); xcere2 = MCBSP_XCERE2_RMK(0); xcere3 = MCBSP_XCERE3_RMK(0); pcr = MCBSP_PCR_RMK( MCBSP_PCR_XIOEN_SP, MCBSP_PCR_RIOEN_SP, MCBSP_PCR_FSXM_INTERNAL, /* SS output (Master) */ MCBSP_PCR_FSRM_EXTERNAL, MCBSP_PCR_CLKXM_OUTPUT, /* TX CLK output (Master) */ MCBSP_PCR_CLKRM_INPUT, MCBSP_PCR_CLKSSTAT_0, MCBSP_PCR_DXSTAT_0, MCBSP_PCR_FSXP_ACTIVELOW, /* SS polarity: Valid when SS goes low */ MCBSP_PCR_FSRP_ACTIVELOW, MCBSP_PCR_CLKXP_RISING, /* TX CLK polarity: Sampling at rising edge of clock */ MCBSP_PCR_CLKRP_FALLING ); MCBSP_configArgs(handle, spcr, rcr, xcr, srgr, mcr, rcere0, rcere1, rcere2, rcere3, xcere0, xcere1, xcere2, xcere3, pcr); return; }
C6713的McBSP配置如下
void init_mcbsp(MCBSP_Handle handle) { Uint32 spcr, rcr, xcr, srgr, mcr, pcr; Uint32 rcer, xcer; /* SPI mode, CLKSTP = 11b and CLKXP = 0: Clock starts with rising edge with delay. */ spcr = MCBSP_SPCR_RMK( MCBSP_SPCR_FREE_DEFAULT, MCBSP_SPCR_SOFT_DEFAULT, MCBSP_SPCR_FRST_DEFAULT, MCBSP_SPCR_GRST_DEFAULT, MCBSP_SPCR_XINTM_DEFAULT, MCBSP_SPCR_XSYNCERR_DEFAULT, MCBSP_SPCR_XRST_DEFAULT, MCBSP_SPCR_DLB_DEFAULT, MCBSP_SPCR_RJUST_DEFAULT, MCBSP_SPCR_CLKSTP_DELAY, /* CLKSTP = 11b */ MCBSP_SPCR_DXENA_OFF, MCBSP_SPCR_RINTM_DEFAULT, MCBSP_SPCR_RSYNCERR_DEFAULT, MCBSP_SPCR_RRST_DEFAULT ); rcr = MCBSP_RCR_RMK( MCBSP_RCR_RPHASE_SINGLE, MCBSP_RCR_RFRLEN2_DEFAULT, MCBSP_RCR_RWDLEN2_DEFAULT, MCBSP_RCR_RCOMPAND_DEFAULT, MCBSP_RCR_RFIG_NO, MCBSP_RCR_RDATDLY_0BIT, /* 0 - (Slave) */ MCBSP_RCR_RFRLEN1_DEFAULT, MCBSP_RCR_RWDLEN1_32BIT, MCBSP_RCR_RWDREVRS_DISABLE ); xcr = MCBSP_XCR_RMK( MCBSP_XCR_XPHASE_DEFAULT, MCBSP_XCR_XFRLEN2_DEFAULT, MCBSP_XCR_XWDLEN2_DEFAULT, MCBSP_XCR_XCOMPAND_DEFAULT, MCBSP_XCR_XFIG_DEFAULT, MCBSP_XCR_XDATDLY_0BIT, /* 0 - (Slave) */ MCBSP_XCR_XFRLEN1_DEFAULT, MCBSP_XCR_XWDLEN1_32BIT, MCBSP_XCR_XWDREVRS_DISABLE ); srgr = MCBSP_SRGR_RMK( MCBSP_SRGR_GSYNC_FREE, MCBSP_SRGR_CLKSP_RISING, MCBSP_SRGR_CLKSM_INTERNAL, /* SRGR clock mode from internal source */ MCBSP_SRGR_FSGM_DEFAULT, MCBSP_SRGR_FPER_DEFAULT, MCBSP_SRGR_FWID_DEFAULT, MCBSP_SRGR_CLKGDV_OF(0) /* C671X: CLKG = CPU/2 / (CLKGDV+1) */ ); mcr = MCBSP_MCR_DEFAULT; rcer = MCBSP_RCER_DEFAULT; xcer = MCBSP_XCER_DEFAULT; pcr = MCBSP_PCR_RMK( MCBSP_PCR_XIOEN_SP, MCBSP_PCR_RIOEN_SP, MCBSP_PCR_FSXM_EXTERNAL, /* set SS as input - (Slave) */ MCBSP_PCR_FSRM_EXTERNAL, MCBSP_PCR_CLKXM_INPUT, /* set TX CLK as input - (Slave) */ MCBSP_PCR_CLKRM_INPUT, MCBSP_PCR_CLKSSTAT_0, MCBSP_PCR_DXSTAT_0, MCBSP_PCR_FSXP_ACTIVELOW, /* SS polarity: Valid when SS goes low */ MCBSP_PCR_FSRP_ACTIVELOW, MCBSP_PCR_CLKXP_RISING, /* TX CLK polarity: Sampling at rising edge of clock */ MCBSP_PCR_CLKRP_FALLING ); MCBSP_configArgs(handle, spcr, rcr, xcr, srgr, mcr, rcer, xcer, pcr); return; }
pcr = MCBSP_PCR_RMK( MCBSP_PCR_XIOEN_SP, MCBSP_PCR_RIOEN_SP, MCBSP_PCR_FSXM_INTERNAL, /* SS output (Master) */ MCBSP_PCR_FSRM_INTERNAL, MCBSP_PCR_CLKXM_OUTPUT, /* TX CLK output (Master) */ MCBSP_PCR_CLKRM_OUTPUT, MCBSP_PCR_CLKSSTAT_0, MCBSP_PCR_DXSTAT_0, MCBSP_PCR_FSXP_ACTIVELOW, /* SS polarity: Valid when SS goes low */ MCBSP_PCR_FSRP_ACTIVELOW, MCBSP_PCR_CLKXP_RISING, /* TX CLK polarity: Sampling at rising edge of clock */ MCBSP_PCR_CLKRP_FALLING );
如上所示,尝试修改了pcr寄存器的FSRM和CLKRM为输出后,
可以收到rrdy信号,但是从端收到的数据完全是错误的
C6416的运行代码
while(1) { MCBSP_write(hMcbsp_Master, 0x050A050A); while(!(MCBSP_xrdy(hMcbsp_Master))); }
C6713的运行代码
while(1) { while(!MCBSP_rrdy(hMcbsp0)); readBuff = MCBSP_read(hMcbsp0); }
6416发送的值是0x050A050A,6713的DRR寄存器的值是0x800000F8,
请问是否还有什么配置是需要注意或修改的?
那这样是不是意味着两片 DSP 的连线应该是
CLKX (6416) - CLKX (6713)
FSX (6416) - FSX (6713)
目前在调试的 pcb 板的连线是
CLKX (6416) - CLKR (6713)
FSX (6416) - FSR (6713)
上述连线状态下是不是可以使用非 SPI 模式的 McBSP 通信协议?
SPI mode连线是你说的这种。
你现在板子的接法就不能用SPI mode,用mcbsp通信协议即可。有代码可以参考。
http://www.ti.com/lit/an/spra455a/spra455a.pdf
问题已解决
硬件工程师本来是想要在整块板上统一使用 SPI 接口协议
但是 DSP 之间的连线不匹配 SPI 模式
改用 McBSP 接口协议很快解决数据收发
谢谢