This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求大神指教下关于vpss dvo2输出的问题



我设置 displayPrm.displayId  = DISPLAY_LINK_DISPLAY_BP1;后出现dcGetResources这个函数报错,导致start display 失败,问下路径有什么问题请指正。

Vps_DcConfig gSystem_dctrlTriDisplayConfig = {
VPS_DC_USERSETTINGS, /* Use Case */
/* Edge information */
{
{VPS_DC_BP1_INPUT_PATH, VPS_DC_HDCOMP_MUX} ,
{VPS_DC_HDCOMP_MUX, VPS_DC_CIG_PIP_INPUT} ,
{VPS_DC_CIG_PIP_OUTPUT, VPS_DC_DVO2_BLEND} ,
{VPS_DC_CIG_PIP_OUTPUT, VPS_DC_HDMI_BLEND},
{VPS_DC_SEC1_INPUT_PATH, VPS_DC_SDVENC_MUX},
{VPS_DC_SDVENC_MUX, VPS_DC_SDVENC_BLEND},
{VPS_DC_GRPX0_INPUT_PATH, VPS_DC_HDMI_BLEND},
{VPS_DC_GRPX1_INPUT_PATH, VPS_DC_DVO2_BLEND},
{VPS_DC_GRPX2_INPUT_PATH, VPS_DC_SDVENC_BLEND},

{VPS_DC_MAIN_INPUT_PATH, VPS_DC_VCOMP},
{VPS_DC_AUX_INPUT_PATH, VPS_DC_VCOMP_MUX},
{VPS_DC_BP1_INPUT_PATH, VPS_DC_SDVENC_MUX},
},

12,
/* VENC information */
{
/* Mode information */
{
{VPS_DC_VENC_HDMI, {FVID2_STD_1080P_60}
}
, /* 1080p30 is mode
* is overwritten
* later inside
* System_displayCtrlInit
*/
{VPS_DC_VENC_DVO2, {FVID2_STD_NTSC}
}, /* 1080p30 is mode
* is overwritten
* later inside
* System_displayCtrlInit
*/

{VPS_DC_VENC_SD, {FVID2_STD_NTSC}
}
}
,
(VPS_DC_VENC_HDMI | VPS_DC_VENC_DVO2), /* Tied VENC bit
* mask */
3u /* Number of VENCs
*/
}
};