This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6614芯片中的BCP数据不同的问题



请教各位一个问题:

    在我们的产品中使用6614中的BCP处理WCDMA基带上行数据,即从AIF获得数据后,依次通过了COR、SSL、DNT、RD这四个子模块,使用BCP的Debug功能记录所有通过模块的包,发现:

    (1)在设备断电重启时,只有1个数据包通过了COR模块,而其他子模块(SSL/DNT/RD)通过的包的个数都为0;与此同时,送入BCP的队列中元素是在不停累积的,直到队列满。

    (2)在设备热重启的情况下,所有数据都是可以通过4个子模块的,设备也是可以正常使用的。

     这是什么原因呢?在网上查说是BCP的SSL死锁了,但又没有给出原因?有没有什么方法在不重启的情况下,解决这个问题呢?谢谢大家~