This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM355 EVM 启动问题



DM355 EVM启动时,一直停留在

Starting demo

Demo interface started at level 0.

进不了文件系统

 

 

 

---------------------------------------boot信息如下-------------------------------------

DM355 EVM # boot

Loading from NAND 1GiB 3,3V 8-bit, offset 0x400000

   Image Name:   Linux-2.6.10_mvl401

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    1585240 Bytes =  1.5 MB

   Load Address: 80008000

   Entry Point:  80008000

DM355 EVM # bootm

## Booting image at 80700000 ...

   Image Name:   Linux-2.6.10_mvl401

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    1585240 Bytes =  1.5 MB

   Load Address: 80008000

   Entry Point:  80008000

   Verifying Checksum ... OK

OK

Starting kernel ...

Uncompressing Linux...................................................................inux version 2.6.10_mvl401 (a0270758@gtmatrix) (gcc version 3.4.3 (MontaVista 3.4.3-25.0.104.0600975 2006-07-06)) #1 Wed Oct 17 15:44:12 EDT 2007

CPU: ARM926EJ-Sid(wb) [41069265] revision 5 (ARMv5TEJ)

CPU0: D VIVT write-back cache

CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets

CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets

Machine: DaVinci DM355 EVM

Memory policy: ECC disabled, Data cache writeback

DM0350

Built 1 zonelists

Kernel command line: mem=116M console=ttyS0,115200n8 root=/dev/mtdblock3 rw rootfstype=yaffs2 ip=off

PID hash table entries: 512 (order: 9, 8192 bytes)

Console: colour dummy device 80x30

Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)

Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)

Memory: 116MB = 116MB total

Memory: 114176KB available (2762K code, 585K data, 164K init)

Mount-cache hash table entries: 512 (order: 0, 4096 bytes)

CPU: Testing write buffer coherency: ok

spawn_desched_task(00000000)

desched cpu_callback 3/00000000

ksoftirqd started up.

desched cpu_callback 2/00000000

desched thread 0 started up.

NET: Registered protocol family 16

Registering platform device 'serial8250.0'. Parent at platform

Registering platform device 'nand_davinci.0'. Parent at platform

Registering platform device 'dm9000.0'. Parent at platform

Registering platform device 'mmc.0'. Parent at platform

Registering platform device 'mmc.1'. Parent at platform

DaVinci I2C DEBUG: 15:42:09 Oct 17 2007

Registering platform device 'i2c'. Parent at platform

SCSI subsystem initialized

usbcore: registered new driver usbfs

usbcore: registered new driver hub

musb_hdrc: version 2.2a/db-0.4.8 [pio] [host] [debug=0]

Registering platform device 'musb_hdrc'. Parent at platform

musb_hdrc: USB Host mode controller at c7800000 using PIO, IRQ 12

musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

arch/arm/mach-davinci/spi_platform_init.c:dm355_spi_board_init:123 dm355_spi_board_init 

arch/arm/mach-davinci/spi_platform_init.c:dm355_spi_board_init:129 REG BOARD  ret 0

Registering platform device 'dm_spi.0'. Parent at platform

arch/arm/mach-davinci/spi_platform_init.c:dm355_spi_board_init:136 REGISTER DEVICE ret 0

NetWinder Floating Point Emulator V0.97 (double precision)

JFFS2 version 2.2. (NAND) (C) 2001-2003 Red Hat, Inc.

yaffs Oct 17 2007 15:41:45 Installing. 

Initializing Cryptographic API

Registering platform device 'dm355fb.0'. Parent at platform

Console: switching to colour frame buffer device 90x30

watchdog: TI DaVinci Watchdog Timer: timer margin 64 sec

Registering platform device 'davinci_pwm0.0'. Parent at platform

Registering platform device 'davinci_pwm1.1'. Parent at platform

Registering platform device 'davinci_pwm2.2'. Parent at platform

Registering platform device 'davinci_pwm3.3'. Parent at platform

Serial: 8250/16550 driver $Revision: 1.90 $ 4 ports, IRQ sharing disabled

Registering platform device 'serial8250'. Parent at platform

ttyS0 at MMIO 0x1c20000 (irq = 40) is a 16550A

ttyS1 at MMIO 0x1c20400 (irq = 41) is a 16550A

ttyS2 at MMIO 0x1e06000 (irq = 14) is a 16550A

io scheduler noop registered

io scheduler anticipatory registered

RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize

loop: loaded (max 8 devices)

dm9000 Ethernet Driver

eth0: dm9000 at c7862000,c7864002 IRQ 45 MAC: 00:0e:99:02:c2:29

i2c /dev entries driver

Linux video capture interface: v1.00

Registering platform device 'vpfe.1'. Parent at platform

vpfe vpfe.1: DaVinci v4l2 capture driver V1.0 loaded

ipipe major#: 253, minor# 0

Registering platform device 'dm355_ipipe.2'. Parent at platform

ipipe driver registered

af major#: 252, minor# 0

Registering platform device 'dm355_af.2'. Parent at platform

aew major#: 251, minor# 0

Registering platform device 'dm355_aew.2'. Parent at platform

elevator: using anticipatory as default io scheduler

at25xxA_spi_eeprom init 

nand_davinci nand_davinci.0: Using 4-bit hardware ECC

NAND device: Manufacturer ID: 0x2c, Chip ID: 0xd3 (Micron NAND 1GiB 3,3V 8-bit)

2 NAND chips detected

nand_bbt: ECC error while reading bad block table

nand_bbt: ECC error while reading bad block table

Creating 5 MTD partitions on "nand_davinci.0":

0x00000000-0x003c0000 : "bootloader"

0x003c0000-0x00400000 : "params"

0x00400000-0x00800000 : "kernel"

0x00800000-0x20800000 : "filesystem1"

0x20800000-0x80000000 : "filesystem2"

nand_davinci nand_davinci.0: hardware revision: 2.3

scan_boardinfo:<NULL>:-1067858964

 modias <NULL> irq 2000000 max_speed 65535 bus_num 0 chip_select 0 mode -1068867824

drivers/spi/spi.cat25xxA_spi_eeprom device register Succeeded

dm_spi.0: dm355 SPI Controller driver at 0xc7866000 (irq = 42)

Initializing USB Mass Storage driver...

usbcore: registered new driver usb-storage

USB Mass Storage support registered.

usbcore: registered new driver usbhid

drivers/usb/input/hid-core.c: v2.0:USB HID core driver

mice: PS/2 mouse device common for all mice

mmc mmc.0: Supporting 4-bit mode

mmc mmc.0: Using DMA mode

mmc mmc.1: Supporting 4-bit mode

mmc mmc.1: Using DMA mode

Registering platform device 'davinci-audio.0'. Parent at platform

NET: Registered protocol family 2

IP: routing cache hash table of 512 buckets, 4Kbytes

TCP: Hash tables configured (established 8192 bind 16384)

Initializing XFRM netlink socket

NET: Registered protocol family 1

NET: Registered protocol family 10

IPv6 over IPv4 tunneling driver

NET: Registered protocol family 17

yaffs: dev is 32505859 name is "mtdblock3"

yaffs: Attempting MTD mount on 31.3, "mtdblock3"

block 649 is bad

block 1645 is bad

block 2449 is bad

block 2884 is bad

block 3309 is bad

block 3970 is bad

VFS: Mounted root (yaffs2 filesystem).

Freeing init memory: 164K

INIT: Entering runlevel: 3

Starting internet superserver: inetd.

ioremap_nocache(0x87500000, 11534336)=0xc7880000

allocated heap buffer 0xc7880000 of size 0x99000

cmem initialized 8 pools between 0x87500000 and 0x88000000

 thttpd

Starting demo

Demo interface started at level 0.