This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

srio测试结果与例程不同



各位专家好!

测试环境:6678+CCSv5.2

使用论坛中例程K1_STK_v1.1中的SRIO程序,进行SERDES_Loopback测试,测试速率5G,参考时钟312.5M(与例程相同),测试结果与例程文档中给出的参考结果不同:

其中每种测试的速率都比例程慢一倍,最高速率1816 Mbps,而参考结果的最高速率为3624Mbps。

请问:1.为什么会出现这种现象呢?

            2.在配置传输速率的过程中,除了参考时钟和传输速率,还需要对其他参数进行配置吗?


以下为板子上跑的部分结果:

[C66xx_0] JTAG ID= 0x1009e02f. This is C6678/TCI6608 device, version variant = 1.

[C66xx_0] DEVSTAT= 0x00001a21. little endian, No boot or EMIF16(NOR FLASH) or UART boot, PLL configuration implies the input clock for core is 100MHz.

[C66xx_0] SmartReflex VID= 63, required core voltage= 1.104V.

[C66xx_0] Die ID= 0x0400300a, 0x04044d3f, 0x00000000, 0x71520001

[C66xx_0] Device speed grade = 1000MHz.

[C66xx_0] Enable Exception handling...

[C66xx_0] SRIO_SERDES_LOOPBACK test start............................................

[C66xx_0] Initialize DSP main clock = 100.00MHz/1x10 = 1000MHz

[C66xx_0] SRIO link speed is 5.000Gbps

[C66xx_0] SRIO path configuration 1xLaneA                       

[C66xx_0] SWRITE   from 0x10802200 to 0x1080a200,      8 bytes,   1110 cycles,    57 Mbps, completion code = 0

[C66xx_0] SWRITE   from 0x10802200 to 0x1080a200,     16 bytes,   1039 cycles,   123 Mbps, completion code = 0

[C66xx_0] SWRITE   from 0x10802200 to 0x1080a200,     32 bytes,   1243 cycles,   205 Mbps, completion code = 0

[C66xx_0] SWRITE   from 0x10802200 to 0x1080a200,     64 bytes,   1279 cycles,   400 Mbps, completion code = 0

[C66xx_0] SWRITE   from 0x10802200 to 0x1080a200,    128 bytes,   1820 cycles,   562 Mbps, completion code = 0

[C66xx_0] SWRITE   from 0x10802200 to 0x1080a200,    256 bytes,   2689 cycles,   761 Mbps, completion code = 0

[C66xx_0] SWRITE   from 0x10802200 to 0x1080a200,    512 bytes,   3814 cycles,  1073 Mbps, completion code = 0

[C66xx_0] SWRITE   from 0x10802200 to 0x1080a200,   1024 bytes,   6054 cycles,  1353 Mbps, completion code = 0

[C66xx_0] SWRITE   from 0x10802200 to 0x1080a200,   2048 bytes,  10427 cycles,  1571 Mbps, completion code = 0

[C66xx_0] SWRITE   from 0x10802200 to 0x1080a200,   4096 bytes,  19343 cycles,  1694 Mbps, completion code = 0

[C66xx_0] SWRITE   from 0x10802200 to 0x1080a200,   8192 bytes,  37245 cycles,  1759 Mbps, completion code = 0

[C66xx_0] SWRITE   from 0x10802200 to 0x1080a200,  16384 bytes,  72897 cycles,  1798 Mbps, completion code = 0

[C66xx_0] SWRITE   from 0x10802200 to 0x1080a200,  32768 bytes, 144323 cycles,  1816 Mbps, completion code = 0

以下为例程文档中给的参考结果:

JTAG ID= 0x1009e02f. This is C6678/TCI6608 device, version variant = 1.

DEVSTAT= 0x00010081. little endian, No boot or EMIF16(NOR FLASH) or UART boot, PLL configuration implies the input clock for core is 50MHz.

SmartReflex VID= 47, required core voltage= 1.001V.

Die ID= 0x02011014, 0x04010169, 0x00000000, 0x40680021

Device speed grade = 1000MHz.

Enable Exception handling...

SRIO_SERDES_LOOPBACK test start............................................

Initialize DSP main clock = 100.00MHz/1x10 = 1000MHz

Initialize DDR speed = 66.67MHzx/1x20 = 1333.333MTS

SRIO link speed is 5.000Gbps

SRIO path configuration 1xLaneA                       

SWRITE   from 0x10802200 to 0x1080a200,      8 bytes,    702 cycles,    91 Mbps, completion code = 0

SWRITE   from 0x10802200 to 0x1080a200,     16 bytes,    807 cycles,   158 Mbps, completion code = 0

SWRITE   from 0x10802200 to 0x1080a200,     32 bytes,    808 cycles,   316 Mbps, completion code = 0

SWRITE   from 0x10802200 to 0x1080a200,     64 bytes,    832 cycles,   615 Mbps, completion code = 0

SWRITE   from 0x10802200 to 0x1080a200,    128 bytes,   1169 cycles,   875 Mbps, completion code = 0

SWRITE   from 0x10802200 to 0x1080a200,    256 bytes,   1612 cycles,  1270 Mbps, completion code = 0

SWRITE   from 0x10802200 to 0x1080a200,    512 bytes,   2129 cycles,  1923 Mbps, completion code = 0

SWRITE   from 0x10802200 to 0x1080a200,   1024 bytes,   3153 cycles,  2598 Mbps, completion code = 0

SWRITE   from 0x10802200 to 0x1080a200,   2048 bytes,   5572 cycles,  2940 Mbps, completion code = 0

SWRITE   from 0x10802200 to 0x1080a200,   4096 bytes,   9866 cycles,  3321 Mbps, completion code = 0

SWRITE   from 0x10802200 to 0x1080a200,   8192 bytes,  18814 cycles,  3483 Mbps, completion code = 0

SWRITE   from 0x10802200 to 0x1080a200,  16384 bytes,  36801 cycles,  3561 Mbps, completion code = 0

SWRITE   from 0x10802200 to 0x1080a200,  32768 bytes,  72333 cycles,  3624 Mbps, completion code = 0