EMMC可以通过SD卡烧录文件系统镜像,但是生产不便,请问如何将编辑好的ext3文件系统烧入EMMC,然后将EMMC焊上板子直接可以运行的。
尝试了下使用EMMC插座插上win7电脑使用win32diskimager软件烧录镜像,但是运行出错。以下是打印信息:
U-Boot SPL 2016.05 (Feb 10 2017 - 00:06:30)
i2c_read (addr phase): pads on bus probably not configured (status=0x10)
tps65217_reg_write failure
i2c_write: pads on bus probably not configured (status=0x10)
tps65217_voltage_update failure
Trying to boot from MMC2
omap_hsmmc_send_cmd: timedout waiting on cmd inhibit to clear
spl: mmc init failed with error: -19
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###
该镜像使用win32diskimager软件烧录到SD卡是可以运行的,当时换成烧录到EMMC就运行不了了,请问有什么区别吗?