This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM437X中ADC1的驱动问题



你好,我在使用AM437X的ADC1是遇到一个问题,我使用 ls -al /sys/bus/iio/devices/iio\:device0/时只能看到

root@am437x-evm:~# ls -al /sys/bus/iio/devices/iio\:device0/
drwxr-xr-x 3 root root 0 Jan 1 2000 .
drwxr-xr-x 4 root root 0 Jan 1 2000 ..
-r--r--r-- 1 root root 4096 Jun 9 20:16 dev
-rw-r--r-- 1 root root 4096 Jun 9 20:16 in_voltage0_raw
-rw-r--r-- 1 root root 4096 Jun 9 20:16 in_voltage1_raw
-rw-r--r-- 1 root root 4096 Jun 9 20:16 in_voltage2_raw
-rw-r--r-- 1 root root 4096 Jun 9 20:16 in_voltage3_raw
-rw-r--r-- 1 root root 4096 Jun 9 20:16 in_voltage4_raw
-rw-r--r-- 1 root root 4096 Jun 9 20:16 in_voltage5_raw
-rw-r--r-- 1 root root 4096 Jun 9 20:16 in_voltage6_raw
-rw-r--r-- 1 root root 4096 Jun 9 20:16 in_voltage7_raw
-r--r--r-- 1 root root 4096 Jun 9 20:16 name
drwxr-xr-x 2 root root 0 Jun 9 20:16 power
lrwxrwxrwx 1 root root 0 Jan 1 2000 subsystem -> ../../../../bus/iio
-rw-r--r-- 1 root root 4096 Jan 1 2000 uevent

没有buffer,scan_elements,mode等文件,请问这是什么导致的?