This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求个TMS320C5517定时器中断的一个例程



新买的开发板,竟然不带任何资料可以学习,只给了网站让人下载。在support.spectrumdigital.com/.../这个网站上下载了个例程,只是简单地几个程序,没有中断使用,而找到的CSL库,在ccs5.5上加载出错,需要ccs6.0以上的版本,但是上面那个网站是用于5.5版本的。求个入门的中断程序。

或者谁知道那个中断矢量表如何写,也就是vectors.asm这个文件如何书写,求告知!

  • 附件是我之前下的ccs v5版本的CSL。

    vectors.asm在C:\ti\c55_lp\c55_csl_3.04\c55xx_csl\src路径下。

  • 非常感谢你的帮助,同时,我想问一下,这个库中不是在ccs_v5.0_examples这个路径下有例程吗,加载完这个例子,并配置好,还需要改啥?

    下面是我编译后出现的错误,不知道是什么原因。

    **** Build of configuration Debug for project timer_interrupt ****

    "E:\\\\ccsv5\\utils\\bin\\gmake" -k all
    'Building file: ../main.c'
    'Invoking: C5500 Compiler'
    "E:/ccsv5/tools/compiler/c5500_4.4.1/bin/cl55" -v5515 --memory_model=large -g --include_path="C:/Users/Administrator/workspace_v5_5/timer_interrupt/include" --include_path="E:/ccsv5/tools/compiler/c5500_4.4.1/include" --define=c5517 --diag_warning=225 --ptrdiff_size=32 --preproc_with_compile --preproc_dependency="main.pp" "../main.c"
    'Finished building: ../main.c'
    ' '
    'Building file: ../lib/csl_intc.c'
    'Invoking: C5500 Compiler'
    "E:/ccsv5/tools/compiler/c5500_4.4.1/bin/cl55" -v5515 --memory_model=large -g --include_path="C:/Users/Administrator/workspace_v5_5/timer_interrupt/include" --include_path="E:/ccsv5/tools/compiler/c5500_4.4.1/include" --define=c5517 --diag_warning=225 --ptrdiff_size=32 --preproc_with_compile --preproc_dependency="lib/csl_intc.pp" --obj_directory="lib" "../lib/csl_intc.c"
    "C:\Users\ADMINI~1\AppData\Local\Temp\0569210", ERROR! at line 1702:
    [E9999]
    Syntax Error
    BIT (ST1,#ST1_INTM) = #1 ;====> CODE AUTO-GENERATED by CSL

    "C:\Users\ADMINI~1\AppData\Local\Temp\0569210", ERROR! at line 1702:
    [E9999]
    Invalid instructionsyntax, Xmem or Ymem expected
    BIT (ST1,#ST1_INTM) = #1 ;====> CODE AUTO-GENERATED by CSL

    "C:\Users\ADMINI~1\AppData\Local\Temp\0569210", ERROR! at line 1702:
    [E9999]
    Invalid mnemonic specified
    BIT (ST1,#ST1_INTM) = #1 ;====> CODE AUTO-GENERATED by CSL

    "C:\Users\ADMINI~1\AppData\Local\Temp\0569210", ERROR! at line 1702:
    [E9999]
    Invalid mnemonic specified
    BIT (ST1,#ST1_INTM) = #1 ;====> CODE AUTO-GENERATED by CSL

    "C:\Users\ADMINI~1\AppData\Local\Temp\0569210", ERROR! at line 1762:
    [E9999]
    Syntax Error
    BIT (ST1,#ST1_INTM) = #0 ;====> CODE AUTO-GENERATED by CSL

    "C:\Users\ADMINI~1\AppData\Local\Temp\0569210", ERROR! at line 1762:
    [E9999]
    Invalid instructionsyntax, Xmem or Ymem expected
    BIT (ST1,#ST1_INTM) = #0 ;====> CODE AUTO-GENERATED by CSL

    "C:\Users\ADMINI~1\AppData\Local\Temp\0569210", ERROR! at line 1762:
    [E9999]
    Invalid mnemonic specified
    BIT (ST1,#ST1_INTM) = #0 ;====> CODE AUTO-GENERATED by CSL

    "C:\Users\ADMINI~1\AppData\Local\Temp\0569210", ERROR! at line 1762:
    [E9999]
    Invalid mnemonic specified
    BIT (ST1,#ST1_INTM) = #0 ;====> CODE AUTO-GENERATED by CSL

    "C:\Users\ADMINI~1\AppData\Local\Temp\0569210", ERROR! at line 1825:
    [E9999]
    Syntax Error
    BIT (ST1,#ST1_INTM) = #1 ;====> CODE AUTO-GENERATED by CSL

    "C:\Users\ADMINI~1\AppData\Local\Temp\0569210", ERROR! at line 1825:
    [E9999]
    Invalid instructionsyntax, Xmem or Ymem expected
    BIT (ST1,#ST1_INTM) = #1 ;====> CODE AUTO-GENERATED by CSL

    "C:\Users\ADMINI~1\AppData\Local\Temp\0569210", ERROR! at line 1825:
    [E9999]
    Invalid mnemonic specified
    BIT (ST1,#ST1_INTM) = #1 ;====> CODE AUTO-GENERATED by CSL

    "C:\Users\ADMINI~1\AppData\Local\Temp\0569210", ERROR! at line 1825:
    [E9999]
    Invalid mnemonic specified
    BIT (ST1,#ST1_INTM) = #1 ;====> CODE AUTO-GENERATED by CSL

    "C:\Users\ADMINI~1\AppData\Local\Temp\0569210", ERROR! at line 1833:
    [E9999]
    Syntax Error
    BIT (ST1,#ST1_INTM) = #0 ;====> CODE AUTO-GENERATED by CSL

    "C:\Users\ADMINI~1\AppData\Local\Temp\0569210", ERROR! at line 1833:
    [E9999]
    Invalid instructionsyntax, Xmem or Ymem expected
    BIT (ST1,#ST1_INTM) = #0 ;====> CODE AUTO-GENERATED by CSL

    "C:\Users\ADMINI~1\AppData\Local\Temp\0569210", ERROR! at line 1833:
    [E9999]
    Invalid mnemonic specified
    BIT (ST1,#ST1_INTM) = #0 ;====> CODE AUTO-GENERATED by CSL

    "C:\Users\ADMINI~1\AppData\Local\Temp\0569210", ERROR! at line 1833:
    [E9999]
    Invalid mnemonic specified
    BIT (ST1,#ST1_INTM) = #0 ;====> CODE AUTO-GENERATED by CSL


    Errors in Source - Assembler Aborted
    16 Assembly Errors, No Assembly Warnings

    >> Compilation failure

    >> Compilation failure
    gmake: *** [lib/csl_intc.obj] Error 1
    'Building file: ../lib/csl_sar.c'
    'Invoking: C5500 Compiler'
    "E:/ccsv5/tools/compiler/c5500_4.4.1/bin/cl55" -v5515 --memory_model=large -g --include_path="C:/Users/Administrator/workspace_v5_5/timer_interrupt/include" --include_path="E:/ccsv5/tools/compiler/c5500_4.4.1/include" --define=c5517 --diag_warning=225 --ptrdiff_size=32 --preproc_with_compile --preproc_dependency="lib/csl_sar.pp" --obj_directory="lib" "../lib/csl_sar.c"
    'Finished building: ../lib/csl_sar.c'
    ' '
    gmake: Target `all' not remade because of errors.

    **** Build Finished ****

  • 还有,问啥我加入这个vectors.asm后,在编译中问啥报语法错误?

  • 试试在ccs->Properties -> C/C++-Build -> Runtime Model Options下面勾选 "Codegen outputs algebraic assembly" ,"Select assembly source language" 选择 Algebraic。