This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dsp c5517 通过mcspi加载程序,但是我发现EBSR SP1MODEBITS RESET DEFAULT 默认的是mmc管脚?

Expert 2137 points
Other Parts Discussed in Thread: TMS320C5517

dsp c5517我以前是通过spi加载的,现在需要 通过mcspi加载程序,但是我发现EBSR SP1MODE Reset Default的状态是MODE0 ,此时的管脚M13 L14 M14 M12 K14 L13对应的是MMC1_CLK、MMC1_CMD、MMC1_D0、MMC1_D1、MMC1_D2、MMC1_D3。而不是对应MCSPI_CLK、MCSPI_CS0、MCSPI_SIMO、MCSPI_SOMI;

这样dsp刚上电时候,我使用mcspi加载,能加载吗?

  • 可以使用mcspi加载模式,配置bootmode管脚为mcspi加载模式1101(10MHz) 或1110(40Mhz)。请看数据手册第75页上的说明。
    5.7.3.4.2 BootMode Implementation and Requirements
    http://www.ti.com/lit/ds/symlink/tms320c5517.pdf

x 出现错误。请重试或与管理员联系。